cancel
Showing results for 
Search instead for 
Did you mean: 

inertial module daisy chain via SPI

Eddess
Associate II

hello

I need to interface about 20 small package inertial sensor via SPI and my MCU doesn't have enough GPIO for the chip selects so I'm looking for a module that can be daisy chained via SPI however I didn't find anything in the datasheets that indicate if these devices are compatible or how to do it.

can anyone tell me if the LSM6DSOX is compatible or if not if there is a module with about the same capabilities that is compatible??

best regards

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Eddess ,

Unfortunately, our IMUs, including LSM6DSOX, require a separate chip select (CS) line for SPI communication.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Eddess ,

Unfortunately, our IMUs, including LSM6DSOX, require a separate chip select (CS) line for SPI communication.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

thanks for the answer. That's indeed unfortunate