MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSO not reading 1G at rest

I  am writing my own library in C++ to operate the LSM6DSO and when the sensor is at rest it reads 0.5 G on the z-axis, I've tried the code with 2 ICs, one in an Adafruit breakout board, and another one in an old PCB that had the sensor soldered one ...

Diogo_Goto_0-1739051739233.png Diogo_Goto_1-1739054006872.png Diogo_Goto_2-1739054522593.png

Temperature characteristics of IIS2DLPC

I am making a simple inclinometer using IIS2DLPC. The 'Zero-g offset change vs. temperature' of IIS2DLPC is specified as a maximum of ±1mg/℃, but some of the boards I made have reached 2.93mg/℃.Some have relatively good values ​​of 0.3-0.4mg/℃, while...

t-susaki by Associate II
  • 574 Views
  • 5 replies
  • 0 kudos

How to write library for LSM6DSOWTR

I am trying to interface LSM6DSOWTR with stm32 using I2c interface. This is the schematic i have made for this module While connecting SD0/SA0 is connected to GND, I have tried to run the I2C scanner and found that it its address is 0x6A but in the m...

Shubham08_0-1741853131591.png
Shubham08 by Associate III
  • 702 Views
  • 2 replies
  • 0 kudos

STEVAL-BFA001V1B wrong cable description

I wanted to try the STEVAL-IDP005V1 from STEVAL-BFA001V1B,I followed the description given in UM2438and nothing worked,Finally I realized that the cable description is wrong (or may be I've got a bad cable),the ground is on white, not on blue wire

MMade.1 by Associate II
  • 1054 Views
  • 5 replies
  • 0 kudos

Using LIS2DH on a SPI bus with many devices

It seems that its CS is inactive, the LIS will assume that it should be in I2C mode.But if I have multiple devices on the SPI bus, then I want to be able to disable I2C mode altogether.Our board has exactly this setup and it seems that whenever I ena...

LSM6DSO32 step count data

Hi, I designed a special board that includes the LSM6DSO32 sensor. I want to get step count data, for testing I am using ESP32-CAM with LSM6DSO32 via I2C. I have followed the basic routine mentioned in application notes. I can get only garbage value....

image.png
rex2 by Associate
  • 409 Views
  • 1 replies
  • 0 kudos

LPS27HHW - Application note how to mount on housing

Hello,I'm looking for any available douments/application notes on how to mount the sensor on a device housing. For example I would like to know what is the suggest o-ring, is it safe to expose the sensor opening to the external world or it needs some...

Resolved! LIS2DE12 coherency in bypass mode

Hi,I am using an LIS2DE12 in I2c mode.  During setup, my code:- wrote 0 to CTRL_REG4 (BDU=0, FS=00, ST=00, and SIM=0)- wrote 0 to CTRL_REG2 (no high-pass filtering)- wrote 0 to CTRL_REG5 (disable FIFO)- wrote 0 to FIFO_CTRL_REG (selects Bypass mode)-...