MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tof Sensor Light intensity

Hi,We are using Tof Sensor VL53L1X in our project.Following are the queries regarding light intensity while measuring distance .1. Dark light means what lumens you consider the light intensity2. If any room is with 1000 lux light intensity than what ...

PVala.1 by Associate II
  • 7553 Views
  • 10 replies
  • 1 kudos

Cannot run the BlueCoin SD demos

Hello,I have recently bought the BlueCoin kit. I have tried some of the demo project from the software library STSW-BCNKT01_V2.3.0, by directly dragging the .bin file into the Nucleo 64 board icon.I'm experiencing issues with SD card demos, where the...

frnt by Senior
  • 4781 Views
  • 12 replies
  • 0 kudos

Resolved! Configuring ASM330LH in Linux

Hi,I am working on ASM330LH in Linux. After enabling ASM drivers, IIO drivers in kernel and adding asm node entry in device tree, the device is getting detected.target:/sys/bus/iio/devices # lsiio:device0 iio:device1 iio:device2 iio_sysfs_triggerBut ...

NM S.1 by Associate
  • 3065 Views
  • 4 replies
  • 0 kudos

Resolved! values ​​of iis3dwb mems

I am reading the x, y, z axis values ​​of iis3dwb mems using DSP Microprocessor.​However, the following results are displayed.lpf or 2g, 4g, 8g, 16g change the sameI want to ask if the procedure is wrong​X auxi : red graphinitial(default) value : 39x...

Kyouk.1 by Associate III
  • 6848 Views
  • 16 replies
  • 1 kudos

3D pose estimation solution based on time of flight (TOF)

This topic aims at the implementation of a self-localization solution for a probe moving through hollow spaces of parts or machines of interest. Here, a small TOF-sensor (time of flight) is to be used and its raw output data to be processed and analy...

Mali.1 by Associate II
  • 1875 Views
  • 3 replies
  • 0 kudos

Hi, I am using LIS3DH in one of the application. What will happen if you read the registers second time after writing the registers? I am reading the registers with I2C multiple bytes, updating only the required bits and writing registers.

 am reading the registers with I2C multiple bytes, updating only the required bits and writing registers. So without power reset if i follow same sequence of reading again and updating only bit values (but writing full register values) then the outpu...

UMahi.1 by Associate II
  • 2230 Views
  • 4 replies
  • 0 kudos

Resolved! Linear acceleration motionfx slope problem?

Hello I am using Lsm6dsox(acc and gyro) and lsm303ah(mag) and sending data to motionfx to calculate the linear acceleration.My sensors are working in mode2 sync with drdy at 104HZ. So I'm reading every 10ms the data from the sensors and sending it to...

suads by Associate III
  • 3978 Views
  • 7 replies
  • 0 kudos