Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
It correctly reads expected values for about 4 hours and then goes to undetected state by SPI. Then IMU does not work even after I reset the microcontroller. IMU only works again after I power off and on the system again. What could be the reason an...
I bought the STEVAL-MKI109V3 motherboard and the STEVAL-MKI196V1 evalboard for the LSM6DSO. Now, i try to use the unico GUI to start working with the LSM6DSO, but I get the attached error message when I select the used components. Further, I tried wi...
Hey guys,I am currently trying to interface a VL6180x to a micro controller and when i try reading the RESULT__INTERRUPT_STATUS_GPIO (0x04f) register i get 0x40 indicating a Laser Safety Error . I checked the documentation and dint find anything of ...
Please Reply Faster....
I'm using sensor LIS2DH12, acceleration data I get looks OK. But I'm bit confused about temperature data.CTRL_REG4.BDU is set to 1CTRL_REG4.FS is set to 0 (= 2g scale)CTRL_REG1.LPEN is set to 0CTRL_REG4.HR is set to 0 (= 10bit normal mode)CTRL_REG1.O...
I am trying to set up interrupt driven reading of X Y Z accelerations and X,Y and Z Gyro data on an ISM330DLCLSM6DSM. The plan is to generate an active high signal on INT2 when data becomes available as signalled by INT2_DRDY_XL (BIT0) of INT2_CTRL ...
Hello, I am developing a feet scanner with the vl6180x sensors. But I need to protect the sensors behind 6mm security glass, patients will step on the glass. When I read behind a 3mm glass, everything works fine, but when I use an 6mm glass the measu...
Dear Sir,Can we use LSM6DS3H measure a tilt angle referenced to Earth? It has 6DOF angular velocity and velocity measurement. Can we combined these 2, do some calculation to measure its tilt angle / static angle. Which mean when unit turn on or...
Dear Concern,we have tried to configure the accelerometer LSM6DSO module through SPI interface using NRF52xx DK board. External Module was not configured properly without minimum nrf_delay_ms(10).Is any reason behind this delay, as it is not working ...