Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,We are currently evaluating the possibility of using the LSM6DSO and LPS22HH with the MotionFD library, to detect when our product has been dropped from height (up to 9 meters).One of our requirements is that the product always monitors for fall e...
I cannot decide which one to use in my application, which is a portable radar fixed to the back of a vehicle. My only requirement is that its orientation is correct when first put in place. Will the LIS2DH12 suffice. I do know that the LIS2DW12 ha...
Hi, I am using LSM6D33 accelerometer sensor. I want to measure vibration and I didn’t find anything this subject. How can I calculate vibration ?
Assembly of the device is extremely tricky since the terminals are all hidden from view and one can never be sure of the correct alignment. Also the terminal 1 is marked only through a notch on the terminal 1 and the dot on the top surface isnt visib...
Hello all, I have a problem when I try to use VL53L0X GUI application: it doesn't recognize the NUCLEO-L476RG board. First, I install STSW-LINK007 and STSW-LINK009 as manual says.Then I connect X-NUCLEO-53L0A1 + NUCLEO-L476RG to my USB port, start th...
The 1 bit PDM data output should be converted to a 16 bit PCM data format using this and what peripherals should be used in STM32cubeMX and the obtained PCM should be converted into .wav file and display it on UART/USARTWhat is the process could anyo...
Hello ST Community,I am using LIS2DH12 sensor for the following purpose: Generate an interrupt when the acceleration exceeds 1.7 g in any axes and read the x, y and z-axis values after the interrupt is generated. Generate an interrupt when the accele...
Please Provide the detailed procedure as I am a beginner to STM32 and do provide the source code and pinout