MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! getting timestamp on tilebox

HelloI know that tilebox has a RTC module, so I realise it is psoible to get current time for generating timestamp for data. Is it posible to do it? Is there any implementation of that in given project examples? Thank you

NMart.1 by Associate III
  • 1654 Views
  • 1 replies
  • 0 kudos

Resolved! Need Certificate of Conformity

Hi,I am using STM32WB55RG as the MCU and LSM6DSO32 as the ACCELEROMETER in my project. In order to get my project CE certified, I require the Certificate Of Conformity for the both components.Hope you guide me to the right path.Thank You and Warm Reg...

PPera.1 by Associate II
  • 9838 Views
  • 11 replies
  • 0 kudos

Resolved! Why the Z axis is noisier than the others axis?

Hi, I'm testing with the LIS3DHTR and I notice that the Z axis is noisier than the others axis. It doesn't matter the position of the accelerometer, always the Z axis is noisier. Why does happen?

AJura.1 by Associate II
  • 6878 Views
  • 10 replies
  • 0 kudos

X-NUCLEO-53L1A2 board doesn't work with VL53L1_GUI. Center is no problem, but other sides (not only LEFT but also RIGHT) didn't work. I purchased two connectors (2x5 box) and soldered them on the board. I connected breakout boards to LEFT and RIGHT.

If I selected CENTER, the measurement started well. But if I selected LEFT or RIGHT, the measurement seemed to be stopped even though start button was pushed. Is it bug?

TYomo by Associate II
  • 1297 Views
  • 1 replies
  • 0 kudos

Resolved! Hi, I have a VL53L1 board, I looked into the datasheets and it got me confused. I have a few questions and it would be very much helpful if u could explain to me.

I cannot understand the term "coverglass crosstalk and smudge beyond 80 cm". Is the glass already in the sensor or does it mean that I can use any glass? Can I program the sensor without setting the preset mode or is it mandatoryThank you so much

MBabu.2 by Associate II
  • 3160 Views
  • 5 replies
  • 0 kudos

Resolved! ADXL3555 Accelerometer with STM32F4

Hi everyone,I am trying to bring in sensor synchronization for accurate data acquisition in a wireless sensor network built using STM32F407 Discovery. ADXL355 Digital accelerometer (shown below ) provides full external sync by applying an external cl...

0693W000006Fj6DQAS.jpg
MHass.2 by Associate III
  • 2723 Views
  • 1 replies
  • 0 kudos

Resolved! How to use the high pass filter in LIS3DHTR?

Hi, I'm using the LIS3DHTR and I read the applications note and the datasheet, but after that I'm still no understanding how to use the high pass filter, so I have some questions.1-The purpose of the high pass filter is to filter de DC component?2-I ...

AJura.1 by Associate II
  • 2778 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.