2020-10-19 10:56 PM
We are using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.
It is observed that the FFT data is not represented in Unicleo-GUI when FFT size is changed from FFT_SIZE_512 FFT_SIZE_1024 in MotionSP_Config.h file.
Please suggest the configuration settings to increase FFT size.
2020-10-21 1:21 AM
Hi @Rajesh , @SS_135 ,
Can I refer here also for to this thread?
In the meantime, I asked internally to our experts.
Meanwhile, for my better understanding, the issue is that you are changing the FFT_SIZE from FFT_SIZE_512 to FFT_SIZE_1024 in MotionSP_Config.h file (in the code section below), but you are not experiencing the related FFT plot in Unicleo-GUI, right? Did you changed the FFT_SIZE_MAX default value?
#define FFT_SIZE_512 512u //!< FFT will be performed on 512 samples
#define FFT_SIZE_1024 1024u //!< FFT will be performed on 1024 samples
#define FFT_SIZE_MAX FFT_SIZE_512 //!< Max FFT size
/* Set parameters for MotionSP library */
MotionSP_Parameters.FftSize = FFT_SIZE_DEFAULT;
MotionSP_Parameters.tau = TAU_DEFAULT;
MotionSP_Parameters.window = WINDOW_DEFAULT;
MotionSP_Parameters.td_type = TD_DEFAULT;
MotionSP_Parameters.tacq = TACQ_DEFAULT;-Eleon
2020-10-21 7:24 AM
Hi Eleon,
Thanks for your response.
We have changed the FFT_SIZE_MAX default value as shown below.
#define FFT_SIZE_DEFAULT FFT_SIZE_MAX //!< Default value for FFT size
.
.
.
//#define FFT_SIZE_MAX FFT_SIZE_512 //!< Max FFT size
#define FFT_SIZE_MAX FFT_SIZE_1024 //!< Max FFT size
The related FFT plot is not shown up in Unicleo-GUI.
Please let us know, if we are missing any other configuration.
Regards,
Rajesh K.
2020-10-26 12:39 AM
Hi @Rajesh , @SS_135 ,
here is our feedback: the project cannot be easily modified to 1024 points.
This because it uses sensor FIFO which has 3kB, so we it is not possible in FIFO standard mode to fit more the 512 samples (512 x 2 bytes x 3 axis). To increase number of FFT points the project would need to be modified to use FIFO compression or to use local buffer and copy samples from FIFO to the buffer, and it is difficult to do it so far...
-Eleon
2020-10-26 1:16 AM
Hi Eleon,
Thanks for your response.
Do you have an example code or application where local buffers are used instead of FIFO to calculate FFT of vibration sensor.
Do you have a generic FFT library instead of MotionSP library to calculate FFT of vibration sensor.
Regards,
Rajesh K.
2020-10-28 11:30 PM
Hi Eleon,
We have verified the data sheet of ISM330DHCX which is used in evaluation board [X-Nucleo-IKS02A1].
The FIFO size is 9K bytes. Please find the captured data below for your reference.
I suggest the changes in vibration monitoring example to use 9K bytes of FIFO, which shall be used to represent FFT data.
Regards,
Rajesh K.
2020-10-29 3:23 AM
Hi @Rajesh ,
>> The FIFO size is 9K bytes. Please find the captured data below for your reference.
Please note that, as reported in the ISM330DHCX datasheet at p. 31:
"the ISM330DHCX embeds 3 kbytes of data (up to 9 kbytes with the compression feature enabled) in FIFO to store the data"
This means that, as I wrote in my last comment, the >3kBytes functionality implies the FIFO compression feature, and it is not the default operation of the sensor.
I reported this suggestion internally. However, since this is a pretty major change in the interface between the Unicleo-GUI and the board(s) firmware, to help speeding up the processing of the request I suggest you to contact a sales representative from your country from this link.
-Eleon
2020-12-04 5:47 AM
Hi Eleon,
Now we are ready with our custom board which has vibration sensor [ISM330DLC] and MCU[STM32F446RE].
We have done following configuration using XCUBE-MEMS1
We have implemented following features
We are using following versions of tools.
Issue:
Regards,
Rajesh K.