MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CUBEMX- Error while Analyzing the model.

Hi ST Member, Am getting the following error while Analyzing the model file in Stm32CubeMx."ImportError: cannot import name 'get_all_providers' from 'onnxruntime.capi._pybind_state' (C:\Users\Systemname\STM32Cube\Repository\Packs\STMicroelectronics\...

Resolved! MotionFX magnetometer calibration not always working

Hi everybody,I use the motionFX with accelerometer, gyroscope and magnetometer (9X sensor fusion) but I have a problem using the magnetometer calibration.I proceed as mentioned in the documentation of motionFX library:Call MotionFX_MagCal_initCall Mo...

BFlor.1 by Associate II
  • 2608 Views
  • 4 replies
  • 0 kudos

Resolved! Set H3LIS331DL to generate continuously Pulse for DataReady Interrupt

Is it really possible to configure H3LIS331DL to fire an interrupt (a pulse) for each DataReady ?I've never succeded in doing that, It seems to be always mandatory to read Acceleration to "release" the interrupt line, hence being able to have a new i...

PGoud by Associate III
  • 2997 Views
  • 4 replies
  • 0 kudos

Resolved! LIS2DW12 and nRF52840 Feather Express via I2C HW issue

I have a simple setup of (Arduino) nRF52840 Feather Express connected to steval-mkiv1-184872 -evaluation board. I was going to use it via I2C bus, and followed the connection diagram almost to last letter.   I connected SDA/SCL to feather   I connect...

I have lsm6dso sensor. I am using fsm interrupt for different events. I have 3 programs in fsm. When the event detected, interrupt comes.I gave three fsm program to same interrupt pin. But I want to know which fsm event detected ?

I have lsm6dso sensor. I am using fsm interrupt for different events. I have 3 programs in fsm. When the event detected, interrupt comes.I gave three fsm program to same interrupt pin. But I want to know which fsm interrupt detected .When I read the ...

Iakgu.1 by Associate III
  • 3169 Views
  • 6 replies
  • 0 kudos

Resolved! STTS22H - I2C Address Setting

Hello,In the data sheet of the sensor (https://www.st.com/resource/en/datasheet/stts22h.pdf), it's mentioned that to set the Address we need to connect the ADDR pin whether to VDD (to have the address 0111000) or to GND (to have the address 0111111),...

OHADD.1 by Associate
  • 2378 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dso fsm filter

I have lsm6dso imu sensor, I can add high pass filter or slope filter for wake-up interrupt.Is it possible to add filter to fsm interrupt ?

Iakgu.1 by Associate III
  • 2671 Views
  • 4 replies
  • 0 kudos