MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Earbuds

Hi Team,I came across the LSM6DSV16BX, which seems suitable for sports earbuds. Are there any compact earbud-style development boards or hearable devices available on the market?

MEMS Acceleromter

Hello,I am looking for MEMS accelerometer for seismic application.We need low noise, up to 100Hz bandwidth, full scale +-2g range.I consider IIS3DHHC as a candidate, which has features as below:3-axis, ±2.5 g full-scaleUltra-low noise performance: 45...

lhagva99 by Associate
  • 632 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dsv and quaternions and direction of a cube/dice

Hi based on the quaternion/Sensor fusion of LSM6DSV example I developed an application where I display the direction of a cube. Everything works fine, no drift, but: when I take the device move and turn it around, then put it back in the same exact p...

MK..1 by Associate III
  • 505 Views
  • 3 replies
  • 0 kudos

LIS2HH12 Interrupt generation

Hello all,I'm currently using the LIS2HH12 to sense the acceleration on the three axes. My aim is not to continuously read the acceleration value, but is to set a threshold for each axis and receive an interrupt when one of the thresholds is exceeded...

GiorgioR by Associate
  • 752 Views
  • 3 replies
  • 0 kudos

LPS27HHW Pick&Place and conformal coating

I'm trying to use the LPS27HHW in a 1 gram wildlife tracking device (water resistance required) and am wondering (a) how pick&place is supposed to pick up the sensor, and (b) how I can apply automated spray conformal coating to the board. I would hav...

tve by Associate II
  • 1276 Views
  • 5 replies
  • 1 kudos

LIS2DH12TR Dimension Discrepancy

Hello, We received LIS2DH12TR bought from distributor source with full label and full lot code.Our QC team checked with measuring equipment, and we found the height is above the max 1.0mm. Is it considered normal phenomenon?   Referring to photo atta...

LWU.31 by Associate II
  • 527 Views
  • 1 replies
  • 0 kudos

Resolved! STHS34PF80TR INT pin Source / Sink capability?

Greetings - what are the recommended maximum current ratings for the INT pin in either Push-Pull or Open-Drain? And FWIW, I was really surprised NOT to find this published in the datasheet...TIA,-Terry

TPhil.3 by Associate II
  • 315 Views
  • 1 replies
  • 0 kudos

LSM6DSO analog anti aliasing

Hi,I would like to confirm if setting LSM6DSO ODR to 6.66KHz and LPF2 to ODR/10 (resulting to 666Hz bandwidth), then setting a FIFO decimation factor of 8 (resulting to 833hz FIFO ODR) will work in preventing aliasing for signals above 417Hz? We have...

adrianT by Associate II
  • 443 Views
  • 2 replies
  • 1 kudos

LSM6dSOX_MLC

Hi All,I am currently working on a health tracker/monitor project that utilizes the LSM6DSOX sensor, interfaced with the nRF5340 platform and running Zephyr. So far, I have successfully implemented tilt and tap detection features.As the next step in ...