MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Filltering on CCA02M2

Hey ST Community,I'm currently trying out the CCA02M2 MEMS microphone board on a NUCLEO-L476RG, using firmware compiled from X-CUBE-MEMSMIC1.The microphones work, but the signal seems to have some heavy filtering. For example:If I record with Audacit...

KRT by Associate
  • 664 Views
  • 0 replies
  • 0 kudos

How to get calibration level for IMU sensor and magnetometer

After soldering process, IMU sensor and magnetometer need to do calibration after power on, such as flip axis, 8 shaped pattern, or real-time calibration.For ST sensor such as LSM6DSV and LIS2MDL, I want to know how to confirm whether sensor has been...

Yansu by Associate III
  • 3400 Views
  • 4 replies
  • 0 kudos

Actual Detection Range and FOV of STHS34PF80?

Hello everyone,I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 met...

mobaid by Associate II
  • 1828 Views
  • 3 replies
  • 0 kudos

STHS34PF80

I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceiling fan to automatically turn the fan ON and OFF based on human presence and motion. However, the sensor is providing continuously varying output values ...

Compatibility STEVAL-MKI227KA Arduino Mirco

Hello,I'm working on an IMU project. I need to measure pitch/roll/yaw rotation in quaternions.For my first test, I am using a STEVAL-MKI227KA connected to an Arduino micro, which already allows me to extract the quaternions.I send the data via I²C.My...

BapDBD by Associate
  • 645 Views
  • 0 replies
  • 0 kudos

Sensortile.box Pro fails verification after programming

Hello,I was having fun with the Sensortile.box Pro I bought a month ago. When I reset the device to its factory settings (SensorTile.boxPRO.bin in file en.stsw-mkboxpro-fs.zip) using the STM32CubeProgramming tool, the device blinks the red LED once a...

cookao by Associate II
  • 6871 Views
  • 5 replies
  • 0 kudos

Resolved! Regarding imp34dt05 mems sensor configuration

Sir,I am working on the imp34dt05 sensor but how could we configure its parameter.Could u guide us for that.What should be sampling frequency and what is the range of the frequency that it can capture and what should be sampling frequency of pcm and ...

Ultra Low Power Mode for LSM6DS032 is not working.

Currently designing a  low power embedded system for monitoring application using IMU LSM6DS032, tried both low power/normal mode and the ultra low power mode setting on this IMU, but I could not find the significant difference in the power consumpti...