MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IMU layout for flex PCB

I am reading through TN0018 and saw that it is possible to have signal and plane on the bottom layer. Does this apply to flex PCB with 50-150um thickness? 

qkieu_0-1754420772882.png
qkieu by Associate
  • 781 Views
  • 1 replies
  • 0 kudos

ASM330LHH - large gyro biases

Hello, We are using the ASM330LHH in a design and are seeing extremely large gyro biases (~250 deg/s). I am trying to figure out what may be causing them; here is some information on the experiment. We collect data while spinning our custom boards (w...

rcoman_3-1754069871175.png rcoman_2-1754069782871.png
rcoman by Associate
  • 423 Views
  • 1 replies
  • 0 kudos

Interfacing MP34DT06 with STM32F401RE Sensor

Hi,I’m using the NUCLEO-STM32F401RE with the X-NUCLEO-CCA02M2 board, which has two MP34DT06 PDM microphones. I want to capture stereo audio using I2S2 and convert it to PCM using the PDM2PCM middleware in STM32CubeIDE.In AN5027 (page 18), a timer is ...

impacts of IIC error injection with IIS2DLPC

For special test case, that directed connected IIC's SCL(LUX_TILT_SCL) to GND and kept for 5mins, will this action hurt or damage IIS2DLPC?IIC worked with 100kbps.Work with IIC. We found that after this action/error injection:Sometimes, the sensor ca...

BBBBBB_0-1753955870719.png
BBBBBB by Associate II
  • 792 Views
  • 6 replies
  • 3 kudos

IIS2ICLX inclination

Hello, I'm looking for a very high precision inclination sensor. I found this IIS2ICLX. I have some questions on the specifications.1) What is the repeatability of the device?2) From the spec sheet, it might seem like the repeatability of the device ...

gio926 by Associate
  • 1276 Views
  • 2 replies
  • 0 kudos

Reading ISM330DHCX with Nucleo Board (SPI3)

Hi,I am trying to read data from my ISM330DHCX using my STM32G491 Nucleo board over SPI3However, I am having trouble understanding the operation of this device, so I would like to explore the answers to the following questions:1) What is the most bas...

Matthew47_1-1753880655726.png

Resolved! Accelerometers comparison

Dear community,I am selecting an accelerometer to use in a project and I am looking for some advice.Essentially I am looking for the highest performance accelerometer (regarding noise) in the STM portfolio.The sensor requirements are: ~±2g scale supp...

dburgt98 by Associate II
  • 4715 Views
  • 10 replies
  • 4 kudos

Check configuration on lsm6dso32

Hi! I inherited a project and we're seeing strange accelerometer values and I'd like to get a sanity check on my configuration. when Idle and flat, I see 1g on Z, 0g on X and Y. When my device is moving I see peaks on many axes beyond 1g, eg 2.5 on X...

ms360_0-1753746022179.png
ms360 by Associate II
  • 613 Views
  • 4 replies
  • 0 kudos

LIS3DH Double interrupts detection

Hi ST guys,I played with the LIS3DH accelerometer options and don't really see difference in interrupts.Can you explain the differences between 6D and no 6D because as per my understanding of AN3308 the AOI + 6D option is position detection which is ...

quick691 by Associate
  • 437 Views
  • 0 replies
  • 0 kudos