MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWB - ODR/ Data rate Calculation

Hi,I'm using IIS3DWB MEMS sensor to get the motor vibration data which will have a bandwidth of 6kHz and need to store it to a 16GB SD cardI'm confused to calculate the data rate, i mean what is the ODR i need to consider?My calculation is :ODR = 266...

LSM6DSL FIFO stops working after fifty-odd reads

Folks,I have an STM32 rigged up via SPI to read gyro data-only from an LSM6DSL. I read it periodically, every 20ms, and for a while it will report back a few hundred samples in FIFO STATUS REG 1 and 2; I empty the FIFO and after another 20ms it repor...

DiBosco by Senior II
  • 1378 Views
  • 2 replies
  • 0 kudos

Resolved! About ASM330LHH BOOT bit

The ASM330LHH datasheet CTRL3_C (12h) says:Note: The accelerometer must be ON. This bit is cleared automatically. This bit is cleared automatically. Does ON for the accelerometer mean that ODR_XL[3:0] in the CTRL1_XL (10h) register is set to a non-ze...

ggob by Associate III
  • 1273 Views
  • 6 replies
  • 0 kudos

Resolved! Connect WBA55CG + LIS2DUX12

Hello everyone, I'm new to both BLE and MEMS sensor. I want to combine 2 examples code as following:STMems_Standard_C_drivers/lis2dux12_STdC/examples/lis2dux12_mlc_activity_mobile.c at master · STMicroelectronics/STMems_Standard_C_drivers · GitHub ST...

Resolved! ST BLE Sensor app no "flow" function

I am completely new to using the STEVAL-MKBOXPRO (Sensor Tile.Box Pro) sensor, and I have a problem accessing some of the functions in the ST BLE Sensor app. I can connect the sensor in the app, but when I try to plot the data within the app, I canno...

bence_g by Associate
  • 1197 Views
  • 2 replies
  • 1 kudos

ASM330LHH OUT_TEMP register value not change

After activating the accelerometer and angular rate sensor, the temperature sensor value does not change and appears to be frozen. What is the cause of this?Is there any countermeasure?

ggob by Associate III
  • 371 Views
  • 2 replies
  • 0 kudos

IIS2DLPC - Tap Detection Above +2g

Hi,I am working on an application where I need to generate an interrupt whenever a tap exceeds a certain acceleration threshold. I have already chose the IIS2DLPC for this purpose.However, on page 58 of the datasheet, in Table 67 for the TAP_THS_Z re...

Jack9 by Associate II
  • 1157 Views
  • 6 replies
  • 0 kudos