cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB - ODR/ Data rate Calculation

Shubha_358
Associate

Hi,
I'm using IIS3DWB MEMS sensor to get the motor vibration data which will have a bandwidth of 6kHz and need to store it to a 16GB SD card
I'm confused to calculate the data rate, i mean what is the ODR i need to consider?

My calculation is :

ODR = 26667 and 3 axis 6 bytes, which becomes 160kb/s and 12.89GB/day precisely, which is a lot of data for a day

Should i consider the ODR to be 2x times the bandwidth (6kHz in this case)?

Also let me know about the raw data and how can i filter out the 6khz frequency data that i need

1 REPLY 1
TDK
Super User

ODR appears to be fixed here at 26.667 ksps. You can decimate samples after you read them, but the data will have some aliasing due to this. Note that -3dB bandwidth is guaranteed up to 5 kHz per the datasheet.

If you feel a post has answered your question, please click "Accept as Solution".