MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MLC Configuration with Standard C Drivers

I have some questions regarding loading machine learning core configurations, specifically onto the lsm6dsox chip but it should be the same across devices. I have generated .ucf and .h files. I've confirmed that the .ucf file works fine when loaded w...

DHou.1 by Associate II
  • 1445 Views
  • 1 replies
  • 0 kudos

Two iss3dwb sensors - can't choose

Hi there fellas, i got me two Steval-Stwincsv1 and i'm now using the HSDataLog. Everything works perfectly when only one of the sensors is plugged on to the Computer. When i plug the second one and start it, one of them start, and ONLY ONE. It seems ...

BRade.1 by Associate II
  • 1330 Views
  • 2 replies
  • 0 kudos

How can i change the of range of IMU sensor

Hi Everyone,I am using STEVAL-MKI182V2 IMU sensor and can able to get the Euler angles of Yaw=360 degrees , Pitch= +- 180 degrees and Roll=+-90 degrees, now i want to get the Roll with range of +- 60 deg how can i get that range, please suggest me.T...

Anil3 by Associate III
  • 1281 Views
  • 3 replies
  • 0 kudos

ISM330DLC CS and OCS_Aux pin states

If the ISM330DLC is connected to two separate dedicated SPI buses (i.e. no other SPI slaves on the bus) can the CS and OCS_Aux pins be connected to ground or do they have to be controlled by their respective SPI masters?

GnR by Associate II
  • 1123 Views
  • 1 replies
  • 0 kudos

Resolved! How to calibrate the sampling rate of the LSM6DSM sensor?

hello.I am using LSM6DSM to collect acceleration and gyro data.Data is being collected at 52Hz using FIFO, but the actual data collected is about 51.2Hz.It is probably caused by the LSM6DSM internal clock being inaccurate. Is there a way to correct t...

HLee.4 by Associate II
  • 1927 Views
  • 2 replies
  • 0 kudos

Resolved! MLC Python scripts: The decision tree generator code in the MLC.ipynb file in the MLC repo throws error out of box

When trying to run MLC.ibynb in the MLC repo (STMems_Machine_Learning_Core/MLC.ipynb at master · STMicroelectronics/STMems_Machine_Learning_Core (github.com)), there is error thrown from the with call stack:generateDecisionTree > printTree > formatTr...

DHou.1 by Associate II
  • 1770 Views
  • 2 replies
  • 0 kudos