cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, This is a questions regarding ISM330DLC In the datasheet, it is mentioned that the linear acceleration sensitivity can change by ±3% for full scale setting ±2g. Is this change the same for other full scale settings like ±4g,±8g,±16g.

KJose.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @KJ.2ose​ ,

Yes, the sensitivity variation is similar for all the accelerometer full scales, so the change is proportional, even if it is declared only at the lower full scale, since this is a parameter fully tested in production (with the related upper and lower limits).

-Eleon

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @KJ.2ose​ ,

Yes, the sensitivity variation is similar for all the accelerometer full scales, so the change is proportional, even if it is declared only at the lower full scale, since this is a parameter fully tested in production (with the related upper and lower limits).

-Eleon