MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM303AGR INT pin not firing

Hi,I am using nordic MCU to operate LSM303AGR magnetometer device. My goal is to get a Z-axis interrupt upon crossing the pre-calibrated threshold.The i2c write and reads are working fine.INT bit of register 64h (INT_SOURCE_REG_M) is responding when ...

GFone by Associate II
  • 2601 Views
  • 4 replies
  • 0 kudos

STM32 Hal Uart RX randomly Freezes using DMA

Hey guys we are using the HAL Uart at 9600 Baud between our Bluetooth Board and Motion Sensor. We are using the DMA in non circular Buffer mode and then we have an actual Circular Buffer the Data goes into after the DMA. We are noticing randomly the ...

KDham.1 by Associate II
  • 2279 Views
  • 2 replies
  • 0 kudos

MLC Configuration with Standard C Drivers

I have some questions regarding loading machine learning core configurations, specifically onto the lsm6dsox chip but it should be the same across devices. I have generated .ucf and .h files. I've confirmed that the .ucf file works fine when loaded w...

DHou.1 by Associate II
  • 1467 Views
  • 1 replies
  • 0 kudos

Two iss3dwb sensors - can't choose

Hi there fellas, i got me two Steval-Stwincsv1 and i'm now using the HSDataLog. Everything works perfectly when only one of the sensors is plugged on to the Computer. When i plug the second one and start it, one of them start, and ONLY ONE. It seems ...

BRade.1 by Associate II
  • 1365 Views
  • 2 replies
  • 0 kudos

How can i change the of range of IMU sensor

Hi Everyone,I am using STEVAL-MKI182V2 IMU sensor and can able to get the Euler angles of Yaw=360 degrees , Pitch= +- 180 degrees and Roll=+-90 degrees, now i want to get the Roll with range of +- 60 deg how can i get that range, please suggest me.T...

Anil3 by Associate III
  • 1298 Views
  • 3 replies
  • 0 kudos

ISM330DLC CS and OCS_Aux pin states

If the ISM330DLC is connected to two separate dedicated SPI buses (i.e. no other SPI slaves on the bus) can the CS and OCS_Aux pins be connected to ground or do they have to be controlled by their respective SPI masters?

GnR by Associate II
  • 1145 Views
  • 1 replies
  • 0 kudos