MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Output type of INT1 pin on ISM330DHCX

Hello,I cannot find any detail about the output type of INT1 pin in the ISM330DHCX datasheet.From what I read about the registers configuration about this pin, I thought that would be a push-pull output, but if I configure an external 10K pull-up to ...

RBors.1 by Associate II
  • 2695 Views
  • 3 replies
  • 0 kudos

Resolved! blueVoice over sensorTile

Hello,I'm working with blueVoice over sensorTile.I downloaded FP-SNS-ALLMEMS2 project version 2.1.0 and also project FP-SNS-ALLMEMS1 in version 4.2.0 and 4.1.0On Android side i'm using ST Ble Sensor app from Play StoreAll of them give me a very bad a...

Fpanz.1 by Associate
  • 3536 Views
  • 6 replies
  • 0 kudos

Resolved! LIS3DHTR, INT1 and INT2, push-pull or open-drain?

Hi.For accelerometer LIS3DHTR, the output signals INT1 and INT2, pins 11 and 9, they are both push-pull (CMOS) outputs? or one of them, or both, have open-drain configuration?For my projects it is better that both INT1 and INT2 be CMOS outputs.Regard...

JPehl.1 by Associate III
  • 1445 Views
  • 1 replies
  • 0 kudos

Resolved! What is the material the membrane is made from on the LPS28DFW?

I've been working with a LPS28DFWTR pressure sensor and noticed it's pretty sensitive to sunlight. As in, the pressure will climb significantly when the sun shines on it. Because the membrane appears to heat much faster than the temperature sensor it...

ch701x by Associate II
  • 3929 Views
  • 6 replies
  • 0 kudos