MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to access STEVAL-STLKT01V1 in STM32CubeMX

I use the following devices and software:STEVAL-STLKT01V1(STEVAL STLCR01V1)ST-LINK/V2/ 01-0STM32CubeIDE 1.9.0STM32CubeMXSTM32CubeProgrammer​I was able to implement SENSING1 on the device, but I can't specify the board on the MX, so I can't train the ...

庫兵.1 by Associate
  • 1118 Views
  • 0 replies
  • 1 kudos

LPS22HH communication failed

In the case of power on, sometimes, the controller failed commnunication with LPS22HH.The controller side accesses LPS22HH in the following order of processing;1 power on2 wait INT_SOURCE (@24h) BOOT_ON = 03 Set the BOOT bit of the CTRL_REG2(@11h) re...

TOMY.OKA by Associate II
  • 1664 Views
  • 2 replies
  • 0 kudos

[LSM6DSL] strange values from fifo

I am using lsm6dsl sensor.using fifo, we continue to receive accel, gyro, and timestamp&step information in units of 18 bytes, but intermittently strange values continue to come in. Can you tell me why?​I think the order of the data accumulated in fi...

jjo.2 by Associate II
  • 2971 Views
  • 4 replies
  • 0 kudos

Resolved! LPS28DFWTR pressure sensor design bug?

I'd like to raise attention of ST staff regarding the LPS28DFWTR pressure sensor and what I believe is a sensor design issue (I hope I'm wrong, because it is an amazing sensor nevetheless!).The original topic was here:https://community.st.com/s/quest...

SSher.3 by Associate III
  • 2839 Views
  • 3 replies
  • 1 kudos

Resolved! Light sensitivity of LPS33HW waterproof pressure sensors

Hi, I have an application that suggests the pressure sensors are very sensitive to sunlight. 1. I have noticed the same behaviour. Can anyone confirm if the sensor experiences a photo-electric effect that amplifies the signal current within the senso...

0693W00000WIA5ZQAX.png 0693W00000WIA5jQAH.png 0693W00000WIA6DQAX.png
NBake.3 by Associate
  • 1557 Views
  • 1 replies
  • 0 kudos

Resolved! Output type of INT1 pin on ISM330DHCX

Hello,I cannot find any detail about the output type of INT1 pin in the ISM330DHCX datasheet.From what I read about the registers configuration about this pin, I thought that would be a push-pull output, but if I configure an external 10K pull-up to ...

RBors.1 by Associate II
  • 2672 Views
  • 3 replies
  • 0 kudos