Skip to main content
Evelina CAMILLERI
ST Employee
November 11, 2022
Solved

Will the ISPU replace the LSM6DSO32?

  • November 11, 2022
  • 1 reply
  • 814 views

..

    This topic has been closed for replies.
    Best answer by Luca SEGHIZZI

    The ISPU IMU products are pin to pin compatible with the LSM6DSO32.

    It is possible to substitute the LSM6DSO32 with the ISM330ISN, but it an industrial product and doesn't

    get to 32g, its full scale is 16g.

    There is the possibility to choose an ISPU product for consumer applications which is the LSM6DSO16IS which has 16g of full scale, but it can't be programmed with the NEAI, only with C language

    1 reply

    Luca SEGHIZZI
    Luca SEGHIZZIBest answer
    Senior
    November 11, 2022

    The ISPU IMU products are pin to pin compatible with the LSM6DSO32.

    It is possible to substitute the LSM6DSO32 with the ISM330ISN, but it an industrial product and doesn't

    get to 32g, its full scale is 16g.

    There is the possibility to choose an ISPU product for consumer applications which is the LSM6DSO16IS which has 16g of full scale, but it can't be programmed with the NEAI, only with C language