MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! blueVoice over sensorTile

Hello,I'm working with blueVoice over sensorTile.I downloaded FP-SNS-ALLMEMS2 project version 2.1.0 and also project FP-SNS-ALLMEMS1 in version 4.2.0 and 4.1.0On Android side i'm using ST Ble Sensor app from Play StoreAll of them give me a very bad a...

Fpanz.1 by Associate
  • 3511 Views
  • 6 replies
  • 0 kudos

Resolved! LIS3DHTR, INT1 and INT2, push-pull or open-drain?

Hi.For accelerometer LIS3DHTR, the output signals INT1 and INT2, pins 11 and 9, they are both push-pull (CMOS) outputs? or one of them, or both, have open-drain configuration?For my projects it is better that both INT1 and INT2 be CMOS outputs.Regard...

JPehl.1 by Associate III
  • 1433 Views
  • 1 replies
  • 0 kudos

Resolved! What is the material the membrane is made from on the LPS28DFW?

I've been working with a LPS28DFWTR pressure sensor and noticed it's pretty sensitive to sunlight. As in, the pressure will climb significantly when the sun shines on it. Because the membrane appears to heat much faster than the temperature sensor it...

ch701x by Associate II
  • 3902 Views
  • 6 replies
  • 0 kudos

Resolved! Can the LSM6DSM replace the LSM6DS3 with no code changes?

We've been using the LSM6DS3 for several years, and are considering a switch to the LSM6DSM. It appears they are pin-compatible, and a superficial look at the register descriptions indicates they could be software-compatible as well, i.e. I could swa...

AAllg.1 by Associate
  • 2216 Views
  • 2 replies
  • 0 kudos

How to read reset values of lsm6dsox ?

Hi,I'm trying to do reset set in my lsm6dsox sensor. (I use stm32wbx, stm32cubeide,bucemx)İ wrote driver functions.When i get to initialization for my single_tap api . i can not get the default value from the sensor register.what can be the reason ?

FOzat by Associate II
  • 2156 Views
  • 3 replies
  • 0 kudos