Skip to main content
jjo.2
Associate II
November 15, 2022
Question

[LSM6DSL] strange values from fifo

I am using lsm6dsl sensor.

using fifo, we continue to receive accel, gyro, and timestamp&step information in units of 18 bytes, but intermittently strange values continue to come in. Can you tell me why?

​

I think the order of the data accumulated in fifo is broken, can it be like that?

All ODRs were same equally.

configuration :

  • XL_ODR_208Hz
  • GY_ODR_208Hz
  • FIFO_208Hz
  • 16g, 500dps
  • XL_ANA_BW_1k5Hz
  • LOW_NOISE_LP_ODR_DIV_100
  • HP_65mHz_LP1_NORMAL
  • BDU Enable

​

/* Output log: TIMESTAMP count */ 

t[0][0]=473000

t[18][7]=473193

t[36][14]=473386

t[54][21]=473579

t[72][28]=473773

t[90][35]=473966

t[108][42]=472806

t[0][0]=1023    <- abnormal

t[18][7]=16777215 <- abnormal

t[36][14]=767   <- abnormal

t[54][21]=255   <- abnormal

t[72][28]=16776704 <- abnormal

t[90][35]=473966  

t[0][0]=475319

t[18][7]=475512

t[36][14]=475705

t[54][21]=475899

t[72][28]=476092

t[90][35]=476285

    This topic has been closed for replies.

    4 replies

    Eleon BORLINI
    ST Employee
    November 17, 2022

    Hi @jjo.2​ ,

    Can you check please if your code is consistent with the one on Github for the FIFO acquisition? It is available for the LSM6DSM, but it is equivalent at LSM6DSL device for this purpose --> lsm6dsm_read_fifo.c

    -Eleon

    jjo.2
    jjo.2Author
    Associate II
    November 18, 2022

    In the example code below, it read fifo as many as the number of patterns through the lsm6dsm_fifo_raw_data_get() function, but my code is reading at once. Can there be a problem in this case?

    /* example code - lsm6dsm_read_fifo.c */

    while (num_pattern-- > 0) {

    lsm6dsm_fifo_raw_data_get(&dev_ctx, data_raw_angular_rate.u8bit, 3 * sizeof(int16_t));

    }

    /* my code */

    lsm6dsm_fifo_raw_data_get(&dev_ctx, data_raw_angular_rate.u8bit, num_pattern*3 * sizeof(int16_t));

    jjo.2
    jjo.2Author
    Associate II
    November 18, 2022

    In the example code below, it read fifo as many as the number of patterns through the lsm6dsm_fifo_raw_data_get() function, but my code is reading at once. Can there be a problem in this case?

    /* example code - lsm6dsm_read_fifo.c */

    while (num_pattern-- > 0) {

    lsm6dsm_fifo_raw_data_get(&dev_ctx, data_raw_angular_rate.u8bit, 3 * sizeof(int16_t));

    }

    /* my code */

    lsm6dsm_fifo_raw_data_get(&dev_ctx, data_raw_angular_rate.u8bit, num_pattern*3 * sizeof(int16_t));