MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MP34DT05-A PDM: increase SAI clock frequency

Hello everyone,I have an application that eventually record some audios and is working fine with a pair of MP34DT01. It works over SAI with a clock of 1.024MHz and a decimation factor of 64 (for the PDM2PCM), leading to an audio frequency of 16kHz.Th...

TVare.1 by Associate III
  • 2367 Views
  • 2 replies
  • 0 kudos

LIS2DH12TR- Not working on 3.3V.

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 1321 Views
  • 1 replies
  • 0 kudos

LIS2DH12TR- Not working on 2.9V and above voltages

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 1514 Views
  • 1 replies
  • 0 kudos

Resolved! How to activate auto-increment for lps25hb?

I'm using a nucleo f401re with a lps25hb. Currently I'm getting very wrong values, this is caused by the reading of the registers. For example when I call the registers of temperature which is composed by two bytes HAL_I2C_Mem_Read(&hi2c1, LPS25HB_I2...

YGail.2 by Associate III
  • 2212 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.