cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO which conditon pin 2 and pin3 should be connected with VDDOR ?which conditon pin 2 and pin3 should be connected with GND? or either of VDDOR and GND is ok

anne
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @anne​ ,

As you can see in the datasheet p.7, if you are working in Mode 1, you don't need these two pins and, since they are configured by default as high impedance, you can connect them either to Vdd or to GND.

0693W00000QLQYKQA5.pngIn general, a good practice would be to connect them to the application processor, so that they can be used in the future for other unforeseen applications.

-Eleon

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @anne​ ,

As you can see in the datasheet p.7, if you are working in Mode 1, you don't need these two pins and, since they are configured by default as high impedance, you can connect them either to Vdd or to GND.

0693W00000QLQYKQA5.pngIn general, a good practice would be to connect them to the application processor, so that they can be used in the future for other unforeseen applications.

-Eleon