Resolved! LPS22 Device ID
HiI try to read the WHO_AM_I register using SPI but I get 0xB3 instead of 0xB1. Is this correct?Regards
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
HiI try to read the WHO_AM_I register using SPI but I get 0xB3 instead of 0xB1. Is this correct?Regards
I am using LSM6DSMTR with a coin cell battery. I have connected the IMU with NRF52810 using a SPI line. Attached the screenshot.When I am observing the power profiler, VDDIO is gradually taking current after the SPI communication (I have used a 100...
Hi!Our incoming inspection unit failed to find any information on LSM6DSLTR device marking. We got parts with 2 lines on it.SF2D code106 Could you please confirm it is a LSM6DSLTR device? Is there date code on it?
I am initializing the 303 with the following code: /* Turn on accelerometer */ WriteRegister(LSM303AGR_CTRL_REG1_A, LSM303AGR_ADDR_WRITE_A, 0x57); x = ReadRegister(LSM303AGR_CTRL_REG1_A, LSM303AGR_ADDR_READ_A); /* Turn on temp sensor and set BDU bi...
Trying to match STM32F4 with LSM303DLHC and I cannot find for i2c addressing mode of type: Master: | ST | SAD + W | SAK | SUB | SAK | SR | SAD + R | SAK | ... any match in the STN32F4 7 or 10 bit addressing modes. I suppose using all those bits it is...
On initial power up of the sensor box then running the sensor app there is a notice for updated firmware. The app then guides the user through the steps of selecting the update and uploading/installing that update, sensortile.box_v332.bin. The progre...
HiHas nobody used the sensor using SPI interface? I have a power up issue, if CS is left floating till processor drive it to zero it seems device start as i2C and micro Dout is shorted to ground.
Q&A - webinar "Anyone can build smarter applications with this intelligent IMU"
Q&A - webinar "Anyone can build smarter applications with this intelligent IMU"