cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, There is a Machine learning core with exportable features and filters for AI applications in LSM6DSV16X. can we use this feature by using ESP32?

FKara.3
Senior
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @FKara.3​, to the community!

You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @FKara.3​, to the community!

You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FKara.3
Senior

Hello Peter,

Thank you for the answer. Yes, that was what I was looking for.

Kindly,

Fehmi