MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About ASM330LHH STATUS_REG

Please tell me about the STATUS_REG for ASM330LHH. I'm using SPI communication. A similar question was posted earlier, but the situation is slightly different.When I ran the same program on 30 board-mounted samples, 29 of them showed a change in STAT...

ggob by Associate III
  • 332 Views
  • 1 replies
  • 0 kudos

LSM6DSOX MLC ActivityStates

Hi Team,  We are working with the LSM6DSOX sensor and integrating it with two different MCUs: nRF5340 and ATSAMD51, using the I2C communication protocol. We have been able to successfully read the device ID, accelerometer data, and gyroscope data. Ad...

LIS2DUX Step Counter - Maximize Battery

Hello, I am working on adding a pedometer to the Sensorwatch project using this chip.I have the step counter working well, and I also have it working with the LIS2DW. Here's a video of it :)The LIS2DW works by sending 12.5Hz worth of data from its FI...

devolov by Associate
  • 435 Views
  • 1 replies
  • 0 kudos

Footprint LPS27HHTW - connection of central GND pin

Hi,according figure 3 in the datasheet, the pin in the middle (let's name it pin 11) is connected to GND, but this pin is missing in table 1.The linked technical note TN0018 advises to avoid any GND/copper/via below the IC (Figure 12).The eval board ...

bjoern_1 by Associate
  • 346 Views
  • 1 replies
  • 0 kudos

what is the junction temperature of the LSM6DSV80XTR

In the datasheet of LSM6DSV80XTR maximum junction temperature is not mention. Maximum junction temperature is required to do the thermal calculation. please any guidance how to obtain the maximum junction temperature till which this IC can work safel...

rohit3 by Associate
  • 297 Views
  • 2 replies
  • 1 kudos

End of Production of MEMS Microphones?

I ordered one of these evaluation boards (https://estore.st.com/en/steval-mic003v1-cpn.html) and by the time I got it and went back to check the documentation now this microphone, and all other MEMS mics, are listed as "Not Recommended for New Design...