MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Customize STWINKT1

Hello everyone. I'm a beginner to STM32 and STWIN. I'm experimenting with the DATALOG2 firmware on STWIN.My question is about customizing this firmware. What I want to do is keep the DATALOG2 functionality as-is, but add an extra feature: when the ac...

Imu by Associate
  • 1128 Views
  • 2 replies
  • 0 kudos

Error in docs for SDDataLogFileX

The SDDataLogFileX example stores the wave file for the digital microphone but in the following docs it wrongly say that it store for the analog microphone :UM2626 at pages 15 (2.1.5) and 30 (2.2.6)FP-SNS-STBOX1_Quick_Start_Guide at page 27

nicolas by Senior II
  • 539 Views
  • 1 replies
  • 0 kudos

LPS28DFW Mechanical Limit

Hello everyone, I plan to use the LPS28DFW barometer to measure the final pressure after a drop from 30 atm. I only need to sense the final pressure within the sensor’s specified working range, but I’d like to know whether exposure to the initial 30 ...

Resolved! Looking for NFC/BLE P2P wearable

My partner and I are creating an app designed for P2P as well as traditional user/vendor interaction. We need a wearable that can create a mutual event on the back end when the two wearables touch or are in close proximity. I see the ST25R3916 or STM...

Resolved! Question About AVG Filtering in LPS28DFW

I have a question regarding how the averaging filter works in the LPS28DFW pressure sensor (AVG[2:0] in CTRL_REG1).I am wondering whether:A) AVG controls internal ADC oversampling for each individual pressure measurement (i.e., multiple internal samp...

Cannot communicate with LSM6DSV with SPI nor I2C

I designed a small PCB for LSM6DSV but I got no signal on SPI-MISO and got NACK on I2C-SDA.I have replaced several chips but all the chips have the same behaviour(no signal reply).I'm very sure the SPI and I2C pins are correctly connected to LSM6DSV....

pansamic_0-1741676602183.png pansamic_1-1741676713794.png pansamic_2-1741676995350.png IMG_20250311_153603.jpg
pansamic by Associate
  • 1333 Views
  • 1 replies
  • 0 kudos

Resolved! Lsm6dsv 9c boot loop after int

 Hi i have a custom lsm6dsv  module  that is getting  a strange result  after 6a 9c then cycles through  int of the imu 9c seem to make it restart its process  and loop it for a for until 6a is back and 9c comes back and does the exact  same process ...

1000002259.jpg