MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with LIS2H12TR accelerometer

hello everyone:I encountered an issue with inaccurate readings when using the LIS2HH12TR Please take a look.First of all, my application scenario: installed on a device, FPGA reads the current position through IIC at all times, without any sudden vib...

Stevesun by Associate
  • 2275 Views
  • 3 replies
  • 0 kudos

Resolved! Is there a datasheet for LSM6DSDTR?

Hello,I have bought one of ST sensors on LCSC. It's called LSM6DSDTR and after it arrived i was looking for details about this sensor but it seems to not exist outside of china. Is there any way i could find more information about this product or may...

dryet by Associate II
  • 3293 Views
  • 4 replies
  • 0 kudos

LIS2DH sometimes does not update the XYZ data

I am using LIS2DH to detect the tilt angle of a vessel. Sometimes the XYZ reading will freeze, and not update anymore, the only way to reset it is to power on/off the system.

che.1 by Associate II
  • 2457 Views
  • 5 replies
  • 1 kudos

MP34DT05-A current consumption

Hi ST team,I use MP34DT05-A microphone in my design and I measure an addition of ~8.5mA to the average consumption current while the microphone is active.The datasheet specifies 650µA consumption in normal mode, and up to 10mA short-circuit current.S...

AZ.2 by Associate II
  • 2269 Views
  • 3 replies
  • 0 kudos

Resolved! How is ST recommending the use of MEMS Accelerometer for Vibration Sensing applications with Sensor Resonant Frequency as low as 2.4kHz for ISM330DCHX & similarly others?

I am surprised to see half of the MEMS sensor datasheet do not mention sensor resonant frequency. Sensor Noise values feel misleading as we have no clue what noise are we going to receive in our shipment. Also, noise levels are not documented well ei...

Chubs by Senior
  • 2277 Views
  • 2 replies
  • 0 kudos