MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I couldn't turn on the Sensortile.box

I have had testing the SensorTile.Box and today I was trying to turn it on to continue testing and dosen't work, leds didn't ligth up and the sensortilebox looks broken. I was trying to reset the sensor (plug in and plug off the battery) and press th...

SAbba.1 by Associate III
  • 1713 Views
  • 1 replies
  • 0 kudos

Problems reading Y and Z axes on the LSM9DS1 magnetometer.

Hi,While trying to calibrate the magnetometer, upon successive failures, I noticed that the values that were read for the Y and Z axes are successively repeated until a different value is read (as can be seen below). It appears that there's some kind...

0693W00000APO4WQAX.jpg
PMach.1 by Senior
  • 2699 Views
  • 3 replies
  • 0 kudos

FFT feature extraction on Unico

Hello, I recently started working with Unico GUI software and I need to do a classification task for soundwaves with already gathered data using the decision tree from the MLC but I would like the classification based on features that can be extracte...

SRodr.4 by Associate II
  • 1490 Views
  • 1 replies
  • 0 kudos

MotionMC calibration process.

Hello everyone. I make some project based on MotionMC and MotionEC libs. It's a magnetic compass which will use inside the cars. Within the MotionMC library, the end device functions properly if calibrated according to section 2.2.5 of the UM2192 man...

ALT.1 by Associate
  • 1278 Views
  • 0 replies
  • 0 kudos

LIS2DTW12 SENSOR IC

Dear Sir/Madam,​I am trying to configure x axis, y axis and z axis in LIS2DTW12 SENSOR IC interfacing with NUCLEO-L476RG microcontroller when board is towards sky direction. These are the values in z axis1.26 in (+-2g configuration), 2.046 in (+-4g c...

ggowd.1 by Associate III
  • 4835 Views
  • 13 replies
  • 0 kudos

Resolved! Is it possible to use the ULTRA LITE DRIVER (SWST-IMG009) for VL53L1X to manage and control the VL53L1 ToF Sensor?

Hi! My name is Vincenzo.Taking a look at the two sensors, I started to believe that they are similar in terms of Architecture, more precisely it seems to me that the VL53L1 has expanded the characteristics of the VL53L1X at the expense of a slightly ...

VNava by Associate III
  • 4161 Views
  • 6 replies
  • 1 kudos