Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello STMicroelectronics Support Team, I am currently working on a development project where I'm utilizing the LIS2DW12 accelerometer. However, I've encountered an issue with the current consumption of the accelerometer on our custom board. I wo...
Is there a way to move between inactive sample rate and regular sample rate with FSMs enabled?I have configurations written from the host microcontroller to the LSM6DSR in which I can enable or disable double tap and enable or disable the FSM(s) in t...
ST(Semiconductor) chip LSM6DSLTR, the website has NOT checked NRND(NOT RECOMMENDED FOR NEW DESIGNS) notice information, how long is the remaining life cycle of this chip?When is the expected date FOR the manufacturer to notify NRND(NOT RECOMMENDED FO...
I have several lsm303agr that with the accelerometer and the magnetometer in power-down mode consume between 40uA and 20uA while others consume about 2uA as indicated on the datasheet.Even if they have this higher consumption, they perform the self t...
Hi,We are using LSM6DSO32 Sensor in our device. For our application we need two things(Should be able to operate in low power),1) Free fall detection (if device falls down, interrupt should be generated)2) Motion detection (if device is in motion/at ...
I have the source code for the Proteus_BLE_CbM app. No docs to explain how it works either. Any example code would be helpful.Thanks
Hello everyone,I need help regarding LIS3MDL magnetic sensor aka compass issue is i am using this sensoron my custom made gps pcb which is then used by my quadcopter the issue is that it works fine at the very start but after few usage when i connec...