MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Customize STWINKT1

Hello everyone. I'm a beginner to STM32 and STWIN. I'm experimenting with the DATALOG2 firmware on STWIN.My question is about customizing this firmware. What I want to do is keep the DATALOG2 functionality as-is, but add an extra feature: when the ac...

Imu by Associate
  • 861 Views
  • 0 replies
  • 0 kudos

LSM6DSV80X gyro offset

I am using the LSM6DSV80X to get roll-pitch-yaw from SFLP and gyro reading. I noticed that the sensor keeps reporting increasing yaw and increasing offset for X axis while at rest even though the data sheet suggests that it should have up to only 1dp...

qkieu_0-1756075772778.png
qkieu by Associate
  • 681 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Presence and motion sensor

 Hello,        In my case, the STHS34PF80 sensor module is powered using I2C communication with the ESP32 module, and I have tested its functionality only up to 2 feet; beyond that, it fails to detect any presence. However, the datasheet indicates th...

Resolved! STATUS_REG of the ASM330LHH

How long does the TDA bit in the STATUS_REG of the ASM330LHH remain “1”?Is the TDA bit itself a latch type and remains “1” until the temperature output register (OUT_TEMP_H/L, 21h/20h) is read?

ggob by Associate III
  • 249 Views
  • 2 replies
  • 0 kudos

Resolved! ASM330LHH CTRL9_XL DEVICE_CONF

It is recommended that CTRL9_XL DEVICE_CONF in ASM330LHH always set this bit to 1 when configuring the device, but when should it be set back to 0? Should it not be set back?

ggob by Associate III
  • 700 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DS3 SPI Bug?

Hello, I use an AT32F403A MCU to connect LSM6DS3 IMU via SPI 4-wire, then I read the WHO_AM_I register at 0x0F. According to the datasheet, the return value should be 0x69, but the chip returned 0x44. Then I repowered the board, and the value seemed ...

Wakkk_0-1756302516517.png Wakkk_1-1756302521207.png Wakkk_2-1756302530679.png
Wakkk by Associate
  • 667 Views
  • 2 replies
  • 2 kudos

Resolved! IIS2DLPC- Tap threshold

Hi,I'm trying to use the least possible threshold for IIS2DLPC tap detection.Is it achieved by setting TAP_THSX[4:0] as 00000b or 00001b?I see that 1 LSB corresponds to FS/32. Does 00000b means the threshold is 0g or some fixed value?If the threshold...

KJose.1 by Associate III
  • 514 Views
  • 1 replies
  • 1 kudos