cancel
Showing results for 
Search instead for 
Did you mean: 

STATUS_REG of the ASM330LHH

ggob
Associate III

How long does the TDA bit in the STATUS_REG of the ASM330LHH remain “1”?
Is the TDA bit itself a latch type and remains “1” until the temperature output register (OUT_TEMP_H/L, 21h/20h) is read?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ggob,

TDA bit remains set (logic “1”) until the temperature output registers are read by the host. Once the temperature registers are read, the TDA bit is automatically cleared by the device to “0” until the next new temperature data is available.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @ggob,

TDA bit remains set (logic “1”) until the temperature output registers are read by the host. Once the temperature registers are read, the TDA bit is automatically cleared by the device to “0” until the next new temperature data is available.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ggob
Associate III

Thank you very much. It is very helpful.
If the TDA bit is not set to “1” even once after 400ms has passed after the sensor is turned on, is it likely that the startup has failed?