cancel
Showing results for 
Search instead for 
Did you mean: 

ASM330LHH CTRL9_XL DEVICE_CONF

ggob
Associate III

It is recommended that CTRL9_XL DEVICE_CONF in ASM330LHH always set this bit to 1 when configuring the device, but when should it be set back to 0? Should it not be set back?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ggob ,

Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @ggob ,

Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ggob
Associate III

Thank you very much. This is very helpful.
Is it necessary to set this bit to “1” before setting it to “1” by operating BOOT or SW_RESET of CTRL3_C?