MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Strange noise distribution for gyro data from LSM6DSOX

When looking at a chart of integrated single-axis gyro data with a completely stationary sensor, I noticed that there are fairly large jumps once in a while.Since this doesn't look like brownian motion with normally distributed steps, I plotted a his...

imu-integration-chart.png raw_hist.png

Resolved! Difference between each mode of pedometer in LSM6DSOX

Hi,I am implementing the pedometer function using LSM6DSOX.According to the driver file provided by ST, there are three different modes to configure. I want to know the difference between them. I cannot find any information in the datasheet.Appreciat...

Jiabin_0-1690953853420.png
Jiabin by Associate II
  • 4251 Views
  • 8 replies
  • 5 kudos

bring up sensors on steval-mki128v6

Hi,When bring up sensors on steval-mki128v6,  for accelerometer and gyro,  read out who_am_i value is 0x6A, which means lsm6dsm. I can use user application to get samples. But I can't find any steval-mki128v6 document online.V5 is lsm6ds3, V7 is lsm6...

lola by Associate
  • 1407 Views
  • 1 replies
  • 0 kudos

IMU sensor LSM6DSV FIFO Timestamp drift

We are observing that LSM6DSV FIFO Timestamp is drifting at a constant rate when Gyro sensor is enabled.Our ImplementationWe are using 6-axis IMU sensor LSM6DSV with st_lsm6dsvx driver from ST GitHub and integrated with OSD32MP157 SiP.We've modified ...

sw_clock _Screenshot 2023-06-14 at 1.18.28 PM.png hw_clock_image.png
farid by Associate II
  • 3908 Views
  • 1 replies
  • 0 kudos

Calculating Analog reference voltage using vref macro

I am using stm32wl55 controller to Calculate Analog reference voltage using vref macro, which is defined as follows:#define __HAL_ADC_CALC_VREFANALOG_VOLTAGE(__VREFINT_ADC_DATA__,\                                          __ADC_RESOLUTION__) \__LL_AD...

Aanchal by Associate II
  • 2507 Views
  • 0 replies
  • 0 kudos

Resolved! Gesture EVK 1.4.0 doesn't communicate with VL53L8CX

Hello,I have a problem with the Gesture Evaluation Kit v1.4.0(EVK from now on) in combination with Nucleo F401RE and VL53L8CX ToF sensor. After uploading the binary file that comes with EVK, the GUI app sees the comport that Nucleo is connected to, b...

VToma.11 by Associate II
  • 1627 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB ODR at selected bandwidth of ODR/4 on LPF2

Hello Community,I am unsure what the ODR will be for the IIS3DWB sensor when we select the bandwidth of ODR/4.Kindly suggest the relationships if available, I did not find any mention in the datasheet except for Table 45.Are there any setting to sele...

Chubs_0-1690607232220.png
Chubs by Senior
  • 2327 Views
  • 4 replies
  • 2 kudos

Not receiving valid PDM data from MP34DT06J

Hi,I have spent the last 2 weeks working on a project with the STM32F102CBT6 that includes the MP34DT06J MEMS microphone, but so far I have been unable to get it to output a valid PDM data stream. I have tried using both the SPI1 in master receive mo...

TomLillie by Associate II
  • 20539 Views
  • 8 replies
  • 0 kudos