cancel
Showing results for 
Search instead for 
Did you mean: 

Which are the embedded features of LSM6DSV16X?

Evelina CAMILLERI
ST Employee
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luca SEGHIZZI
Senior

LSM6DSV16X has an enhanced AI in-the edge with machine-learning core (MLC), Final state machine (FSM)), while for local processing has a sensor fusion low-power algorithm, an on-the-fly self-configuration, pedometer and an electrostatic sensing (Qvar). These advanced MEMS sensors drive the intuitive context-aware features of today’s battery-operated applications.

View solution in original post

1 REPLY 1
Luca SEGHIZZI
Senior

LSM6DSV16X has an enhanced AI in-the edge with machine-learning core (MLC), Final state machine (FSM)), while for local processing has a sensor fusion low-power algorithm, an on-the-fly self-configuration, pedometer and an electrostatic sensing (Qvar). These advanced MEMS sensors drive the intuitive context-aware features of today’s battery-operated applications.