cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure the sensor fusion low power?

Evelina CAMILLERI
ST Employee
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luca SEGHIZZI
Senior

The SFLP block is enabled by setting the SFLP_GAME_EN bit to 1 of the EMB_FUNC_EN_A embedded functions register. When enabled, it works at a configurable output data rate (which must be equal to or less than the selected output data rates of the accelerometer and gyroscope) through the SFLP_GAME_ODR_[2:0] field of the SFLP_ODR embedded functions register. Finally, the FIFO must be configured to store the SFLP game rotation vector, the gravity vector and/or the gyroscope bias. More details can be found in the AN5763.

View solution in original post

1 REPLY 1
Luca SEGHIZZI
Senior

The SFLP block is enabled by setting the SFLP_GAME_EN bit to 1 of the EMB_FUNC_EN_A embedded functions register. When enabled, it works at a configurable output data rate (which must be equal to or less than the selected output data rates of the accelerometer and gyroscope) through the SFLP_GAME_ODR_[2:0] field of the SFLP_ODR embedded functions register. Finally, the FIFO must be configured to store the SFLP game rotation vector, the gravity vector and/or the gyroscope bias. More details can be found in the AN5763.