MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS28DFW bias stability / difference with other LPS28DFW

Hi,I have two LPS28DFW in my application. The absolute value as well as the difference is important here. I noticed that there is a difference of around 30 Pa. Is it reasonable to assume that this difference is roughly constant in the future? I teste...

LSM6DSV16X drift issue

Hi!We are a group trying to get reliable rotation data out of the LSM6DSV16X sensor. The accumulated error values in the datasheet seemed promising. However, we are currently in a state, where the sensor is returning gyroscope data, but the actual ob...

Gorbit99 by Associate III
  • 4601 Views
  • 5 replies
  • 2 kudos

ISM330DLC, no accelerometer or gyroscope data in FIFO

Greetings,I have been trying to read the sensors from the ISM330DLC using its FIFO. However, when reading the number of samples (FIFO_STATUS1/2), it remains 0 with just dataset 1 and 2 enabled. When enabling dataset 4 with either, or and temperature ...

Asm330 low frequency behavior

Hi I have a questionI am using asm330lhh gyroscopeThe sensor is great but I see some kind of low frequency behavior in the data from this sensorMy ODR is 6667 range is 500The accuracy is good, but this low frequency behavior will eventually cause pro...

image_20230804_231800a997c2ca-dcd2-4cf8-aac5-0027bd9d4e55.jpg image_20230804_231805a044cff2-b268-48bb-a6d7-c22c7c3f092e.jpg
AHass.5 by Associate II
  • 2065 Views
  • 3 replies
  • 0 kudos

ASM330LHB-Query

 Dear team,I'm using ASM330LHB for Electronics Brake control project.Please clarify my queries to use this ASIC in our application.How the ASIC is claimed as ASIL-B? Is there any redundancy in the ASIC itself?How the error detection and error reactio...

ganand05 by Associate
  • 1688 Views
  • 2 replies
  • 0 kudos

pdm2pcm, pcm data noisy , pdm mic nucleo f413zh

hello tout le monde, im worknig on audio project im trying to get data from a pdm microphone as pcm 8 bit and transmit the data via uart  as binary but when i transfer the data from binary to audio via audacity i can hear just noise nothing else, als...

zohbou1 by Associate
  • 2218 Views
  • 1 replies
  • 0 kudos

Resolved! Strange noise distribution for gyro data from LSM6DSOX

When looking at a chart of integrated single-axis gyro data with a completely stationary sensor, I noticed that there are fairly large jumps once in a while.Since this doesn't look like brownian motion with normally distributed steps, I plotted a his...

imu-integration-chart.png raw_hist.png

Resolved! Difference between each mode of pedometer in LSM6DSOX

Hi,I am implementing the pedometer function using LSM6DSOX.According to the driver file provided by ST, there are three different modes to configure. I want to know the difference between them. I cannot find any information in the datasheet.Appreciat...

Jiabin_0-1690953853420.png
Jiabin by Associate II
  • 4166 Views
  • 8 replies
  • 5 kudos