MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can i use STEVAL-MKI208V1K standalone ?

I have STEVAL-MKI208V1K but not its own compatible motherboard. I want to use IIS3DWB sensor. When i connec SDA, SCL, GND and VDD(for vdd i have tried 3v3 and 5v), HAL_OK said HAL_ERROR. Is this STEVAL-MKI208V1K can be used standalone or no? Thanks f...

bcryhun by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos

IIS2MDC

Hi,My thesis topic is to develop a dynamic preventive maintenance schedule for medical devices based on their usage. For this purpose, I have been collecting data using a magnetometer sensor (, we use IIS2MDC) 24/7 for the past 3 months. I need guida...

ABulu.2 by Associate II
  • 1503 Views
  • 1 replies
  • 0 kudos

Resolved! ST sensor - LPS27HHTW pressure read out problem

I would like to read out the pressure reading from this sensor, but it keep returning '0' Status.Tools: Nucleo-767ZI, STM32CUBEIDE, STEVAL-220VI (the sensor eval)I connect Sensor VDD to 3.3V,CS pin to VDD_IO,SDA, SCL pulled up by 4kOhm to 3.3V,INT/DR...

Wai Siang by Associate III
  • 3842 Views
  • 6 replies
  • 3 kudos

Resolved! Marking code

Hi ST Team,Can you share the Marking code specification for the product: LPS22DFTR ?Thanks, Danny.

DNguy.8 by Associate II
  • 7233 Views
  • 11 replies
  • 0 kudos

Resolved! LSM6DSO32 ultra low power mode not working

Hello,I am using a LSM6DSO32 on a custom board.  As an attempt to save power in sleep mode we want to place the device in ULP (ultra low power mode) as specified by the datasheet.  I have attached my function that initializes the device in ULP mode a...

SDZELL18 by Associate II
  • 3276 Views
  • 4 replies
  • 1 kudos

STEVAL-STWINKT1B is not connecting to wifi

Hello. I made all the adjustments for my STEVAL kit. I also installed the necessary binary file in the Wifi module (Dsh predmnt). According to the guide I gave in the link, I stay on page 12 step 8. When I enter the wifi id password, it does not conn...

bcryhun by Associate II
  • 2170 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSL Linux driver, Temperature reading not implemented

Hi Everyone, Below Linux driver for LSM6DSL device has no method to read the temperature sensor. https://elixir.bootlin.com/linux/latest/source/drivers/iio/imu/st_lsm6dsxIs there a complete Linux driver which reads the temperature as well?thanks,   

RAlma.1 by Associate III
  • 3069 Views
  • 4 replies
  • 2 kudos