MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DS3 returning Register address instead of value on most registers

I have multiple LSM6DS3 (with SH SMD markings) and all of them show the same strange behavior.The chip is soldered to a breakout board that is set up on a breadboard. And is connected to the MCU breakout with 20 cm jumper wire.1. When I read a regist...

Maglog by Associate II
  • 3442 Views
  • 6 replies
  • 1 kudos

ST LSM6DS3TR-C Gyro LP Filter

The LSM6DS3TR-C datasheet "Gyroscope LPF1 bandwidth selection" table mentions BWs for 800Hz, 1.6kHz, 3.3kHz and 6.6kHz ODRs. In the same datasheet, the "Gyroscope ODR configuration setting" table lists ODRs of 12.5Hz, 26Hz, 52Hz, 104Hz, 208Hz, 416Hz,...

ISM330DHCX gyro noise at high shock and vibration

Hi,I'm using an ISM330DHCX in a couple of boards.The output looks great on the desk but when subject to high shock and vibration the gyro signal shows a lot of noise (to the point where the rotation value is lost).Is this just something that happens ...

jcslb by Associate
  • 1978 Views
  • 2 replies
  • 0 kudos

LSM6DSRX for angle measurements

I am currently working on a project that involves angle measurement, and I'm using the LSM6DSRX sensor in conjunction with an STM32 microcontroller. I have encountered some challenges, and I would greatly appreciate your expertise and guidance to hel...

SensorTile

At the moment I am making an application for 3D sound detection, in which I am making use of the STEVAL-STWINKT1B and the STEVAL-STWINMAV1 microphone array (which I haven't used yet). I am just starting, and I can not understand the operation of the ...

SAbba.1 by Associate III
  • 11512 Views
  • 7 replies
  • 0 kudos

Resolved! Max Shock/Vibration Survivability for Gyro Sensors

I'm looking for a mechanical survivability spec for shock/vibration for the gyroscope MEMs sensors offered by ST, and was wondering if this information is available somewhere?Specifically interested in the A3G4250D and I3G4250D sensors. Is this infor...