Question
STEVAL-STWINKT1B simultaneous aquisition of 8 mems microphones and logging to SD card
I have been looking at the STEVAL-STWINKT1B sensor tile and the X-CUBE-MEMSMIC1 library. Is it possible to record 8 mems microphones to SD card with this board? I need phase coherence for array processing. All the examples seem to be a maximum of 4 microphones.
I could use analogue or digital microphones. It would be nice to store PCM data on the SD card but I could do the decimation from PDM recordings on a PC along with the array processing.