MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Compensation in temperature for LIS2DW accelerometer

HelloWe use a LIS2DW12 accelerometer to mesure tilt over a temperature range from -25°C to +70°C.We set the full scale to 2g and chose High Performance mode with Low Noise enabled.We want an accuracy of 0.5°, but we're observing a drift of the order ...

LIS331DL SPI communication issue

Hi guys,   I met a SPI communication issue about LIS331DL. The type of kit board is MKI153. When I tied VDDIO and VDD to 3.3V, the data from chip register by SPI isn't correct. When I only connect VDD to 3.3v, The data  is correct.     The register i...

TommyMao by Associate
  • 2043 Views
  • 2 replies
  • 0 kudos

Using LIS25BA with STM32L4 Nucleo Board

I am using STM32L452RE Nucleo Board and LIS25BA module.I2C works fine. I wish to get accelerometer data through TDM now. I am unable to do so. For now, I am using polling mode. The code I am using is given below and the SAI configuration I am using i...

Arka by Associate
  • 3527 Views
  • 2 replies
  • 0 kudos

Resolved! PDM2PCM and I2S Data Frame relation

Dear @Eleon BORLINI​ ,I’m currently using the I2S peripheral to acquire from a digital microphone.The I2S is configured as:24bits on 32bit data frame22kHz sampling frequencyand the pdm library is correctly configured and I’m able to convert a single ...

frnt by Senior
  • 6116 Views
  • 9 replies
  • 0 kudos

iis3dwb唤醒中断无法实现

初始化寄存器的参数配置SPI_write_reg(FIFO_CTRL4, 0x00);//fifo——mode// SPI_write_reg(INTERRUPTS_EN, 0x00);//interSPI_write_reg(CTRL3_C, 0x05); //high_act no_resetSPI_write_reg(CTRL1_XL, 0xA4); //full_scaleSPI_write_reg(CTRL3_C, 0x04); //high_act no_resetSPI_write...

THSW by Associate II
  • 2031 Views
  • 4 replies
  • 0 kudos

Resolved! STEVAL-MKI109v3 COM port not detected

Hi,I have STEVAL-MKI109v3 board and steval-mki186v1 sensor. I have connected the sensor to the board and if I connect the board to my laptop, the laptop is not able to detect the COM port of the board which is connected. It is not detecting the board...

AV B.1 by Associate II
  • 3837 Views
  • 5 replies
  • 0 kudos

Resolved! LIS3DH consuming high current at interrupt

I am using a LIS3DH and I have configured a threshold interruption and it is consuming around 3mA while the interrupt is active. I have very strict power constraints and this consumption make it unreliable.I am using the driver implemented in Zephyr ...

SensorTile.box PRO SWD not connect target!!!

Hi, I purchased the SensorTile.box PRO sensor, but I can't develop because it doesn't connect to the STLINK V2-1, in the datasheet it says:I connect adapter STEVALMK1 (that was inside the kit) with STLINK V2-1But I have the following error  the docum...

1.jpg 2.jpg