LIS3DH consuming high current at interrupt
- October 9, 2023
- 2 replies
- 1772 views
I am using a LIS3DH and I have configured a threshold interruption and it is consuming around 3mA while the interrupt is active. I have very strict power constraints and this consumption make it unreliable.
I am using the driver implemented in Zephyr and it have all configuration from the interrupt exactly as advised in the datasheet, the INTx_SRC is read after a interrupt to clear it and the interrupt is cleared, although the interrupt only is pulled down after a new sample. It is possible to be noticed in the attached file that it takes around 20 ms to put the interrupt to 0. It matches with the sampling period that is 20ms (freq 50Hz).
Why does LIS3DH consumes so much power for keeping the interrupt ON? And is it right to be waiting a new sample to be able to turn down the interrupt?
Is it a problem from LIS3DH or am I missing some config?
Best regards