MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPS33HW and LPS27DFW

Hello,Please, for a pressure measurement in an environment of dust and humidity, which sensor between the 2 you recommend as well as what is the IP protection rating of each sensor.Thanks in advance

ljm by Associate III
  • 1359 Views
  • 1 replies
  • 0 kudos

LSM6DSL Self Test Thresholds

I have performed the self-test on LSM6DSL and observed that it was noted the thresholds mentioned in the datasheet I want to know how these values of  90mg > xxx < 170mg  & 150 dps> xxx <700dps measured?Why does the acceleration and gyro change when ...

RamanaKumar_0-1705576951766.png

LSM6DS3 FTH or FIFO_FULL flags used as ISR

Hi,I am using steval MKI160V1 coupled with pybv1.0 under microphyton (spi speed 525000bits/s).I'd like to get every samples from gyro and accel at 1666 hertz speed using interruption.I have configured lsm6ds3( whoami = 69h) to do so, but while I am f...

L77d by Associate II
  • 1542 Views
  • 2 replies
  • 0 kudos

Resolved! Typo in DS13431 - Rev 3 (ILPS22QS datasheet)

Hi,There is a typo in in the datasheet of the ILPS22QS datasheet: DS13431 - Rev 3.Table 19 on page 32 states that default value of CTRL_REG2 is 00h.But on page 39, chapter 9.7 CTRL_REG2 bit EN_LPFP has a default value of 1 resulting in 10h  I hope th...

Girardey_1-1705351034907.png Girardey_2-1705351161928.png
Girardey by Associate
  • 1109 Views
  • 1 replies
  • 1 kudos

Resolved! lsm6dsr sensor motion information

Hello everyone, I am working with the lsm6dsr sensor. How can I solve the position information or how much I move with this sensor? I am looking at projects with examples on github, but I could not find how to solve the directions, how much the senso...

LSM6DSOX Example

Hi, I'm developing a project with a NUCLEO-WB55RG and I need to to communicate with a STEVAL-MKI197V1. I'm using the CUBE IDE v1.13.1 and the X-CUBE-MEMS1 v10.0.0. But I'm having a problem when trying to initiate the library calling LSM6DSOX_Init fun...