MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DU12TR accelerometer

Hi.  I used LIS2DU12TR accelerometer IC on the PCB.  It's angle value  was changing every sec. but my smart phone app indicated current angle is 0.0 degree.    current angle is -0.515648[proc_bt_read_all] TX data (len=15)00 00 02 00 00 00 00 00 00 7F...

LogosLEE by Associate
  • 3233 Views
  • 4 replies
  • 0 kudos

About MotionFx library

I want to calculate the displacement using the MotionX library with the LSM6DSR sensor on the stm32. For example, I want to write a code that calculates the displacement when the sensor moves 20 cm to the right on the table or calculates the displace...

h3lis200dl consumes too much power.

When I used the IIC communication mode of h3lis200dl, I connected the 7th pin SDO directly to the ground. Since the SDO pin has a pull-up resistor inside, the current is too large (about 60uA). I would like to ask if there is an unopened register to ...

132.png
Phoenix1 by Associate
  • 1724 Views
  • 3 replies
  • 0 kudos

How to store/resotre calibration data?

I'm using lsm6dsv, and must calibrate IMU everytime after power on. Can I read calibration data once, and restore to IMU without calibration?

Yansu by Associate III
  • 1688 Views
  • 2 replies
  • 0 kudos

Read number of unread samples in FIFO - LIS2DW12

GreetingsI am working with the LIS2DW12 accelerometer and I am struggling to read from, and use the FIFO in single-conversion mode, using i2c. The chip is on a dev board which can only be used with i2c, and the INT1 or INT2 pins are not available for...

ZAIDS-S23 by Associate III
  • 3390 Views
  • 3 replies
  • 0 kudos

High Frequency Noise From STWINMA2A

Hello everyone,I am currently working with STWIN+STWINMA2A microphone array for ultrasonic signal processing. I use the firmware "AMicArray_Microphones_Streaming" and connect the board directly to my laptop as an USB microphone.However, the data suff...

xiaohangz_0-1704828877639.png xiaohangz_1-1704828956551.png