BlueCoin入门套件
BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊
Hello,I have run into an unexpected problem when trying to read registers from the IIS3DWB sensor. The setup is attached in the picture. I am using an Arduino Uno R3 and an STEVAL MKI208V1 board. The code is fairly simple so I am not sure what is goi...
Hello ST community,I am unfortunately facing a problem with the MP34DT05-A MEMS microphone. I am using the DFSDM module to read in the microphone. Unfortunately, it happens again and again that extremely strong noise is added at a random time (see pi...
Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?
Hi ST-Team,We want to use the STHS34PF80 for presence detection. I am not very familiar with the sensor, as a just watchedthe webinar about the sensor last Tuesday.I think a good way to check the capabilities of the sensor is the STM32 Open Developme...
Dear ST Team,Greetings. I'm currently employing the ST ISM330DLC accelerometer and gyrometer in my application.I've noticed some unusual readings when the gyrometer is stationary, and I would like to inquire whether this is expected behavior.I've opt...
Hi, I developed lsm6dsv driver on Android CHRE framework. In Android CTS test, some items failed, the reason is "LSM6DSV Gyro Standard deviation out of range: stddev=(0.004091, 0.001167, 0.000378) (expected (0.003456, 0.003456, 0.003456))". How to fi...
We have been using I3G4250DTR for 5 years in our production parts. We have been noticing some recent issues with the I3G4250DTR in that some boards are not sending data (DRDY) at all, or the data is intermittent (less than the 100 Hz data rate). It i...
I'm trying to get the Activity/Inactivity interrupt generation on the LSM6DSL working. I've implemented the example code in the data sheet below. I'm using an stm32L475.However, this interrupt fires constantly, regardless of either the sleep duration...
Hello, can anyone please tell me the part number for a device marking with "SE"? I attached a photograph. Our BOM specifies ST IMU iNEMO parts LSM6DS3TR-C and LSM6DSLTR. The part marked with "SE" is not working like other parts marked with "SH" on...