cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV Gyro Standard deviation out of range

lemon923
Associate II

Hi, I developed lsm6dsv driver on Android CHRE framework. In Android CTS test, some items failed, the reason is "LSM6DSV Gyro Standard deviation out of range: stddev=(0.004091, 0.001167, 0.000378) (expected (0.003456, 0.003456, 0.003456))". How to fix this?

Thank you~

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Joe WILLIAMS
ST Employee

Hello Lemon923

 

Your case is being reviewed through ST's Online Support System now.

 

Kind Regards

Joe WILLIAMS

STMicro Support

View solution in original post

4 REPLIES 4
lemon923
Associate II

I also observed a strange phenomenon, when I turned on the accel, gyro data changed.  Pls refer to the following table,

[4] = -0.001198, 0.000000, 0.000000 @ 11339944704390
[4] = 0.000000, 0.000000, 0.000000 @ 11340078227965
[4] = -0.001198, 0.000000, 0.000000 @ 11340211751678
[4] = -0.001198, 0.000000, 0.000000 @ 11340345273735
[4] = 0.000000, 0.000000, 0.000000 @ 11340478797192
[4] = -0.001198, 0.000000, 0.000000 @ 11340612320430
[4] = -0.001198, 0.000000, 0.000000 @ 11340745843887
[4] = -0.002463, -0.001198, -0.001198 @ 11341146402915 -----> turn on accel sensor
[4] = -0.002463, -0.001198, 0.000000 @ 11341279937651
[4] = -0.002463, -0.001198, -0.001198 @ 11341413467508
[4] = -0.002463, -0.002463, -0.001198 @ 11341546991091
[4] = -0.002463, -0.001198, -0.001198 @ 11341680518836
[4] = -0.002463, -0.001198, -0.001198 @ 11341814036019
[4] = -0.002463, -0.002463, -0.001198 @ 11341947561204
[4] = -0.002463, -0.001198, -0.001198 @ 11342081078451
[4] = -0.002463, -0.002463, -0.001198 @ 11342214602228
[4] = -0.002463, -0.001198, -0.001198 @ 11342348127603
[4] = -0.002463, -0.001198, -0.001198 @ 11342481651572
[4] = -0.002463, -0.001198, 0.000000 @ 11342615173404
[4] = -0.002463, -0.001198, 0.000000 @ 11342748696733
[4] = -0.002463, -0.001198, -0.001198 @ 11342882220965
[4] = -0.002463, -0.001198, -0.001198 @ 11343015744294
[4] = -0.002463, -0.001198, -0.001198 @ 11343149265265
[4] = -0.002463, -0.001198, -0.001198 @ 11343282788594
[4] = -0.002463, -0.001198, -0.001198 @ 11343416310347
[4] = -0.002463, -0.001198, -0.001198 @ 11343549833420
[4] = -0.002463, -0.001198, -0.001198 @ 11343683353752
[4] = -0.002463, -0.001198, -0.001198 @ 11343816876185
[4] = 0.000000, 0.000000, 0.000000 @ 11344083926951 -----> turn off accel sensor
[4] = -0.001198, 0.000000, 0.000000 @ 11344217453111
[4] = -0.001198, 0.000000, 0.000000 @ 11344350977112
[4] = 0.000000, 0.000000, 0.000000 @ 11344484499959
Joe WILLIAMS
ST Employee

Hello Lemon923

 

Your case is being reviewed through ST's Online Support System now.

 

Kind Regards

Joe WILLIAMS

STMicro Support

Hi Joe,

Please feel free to leave a message if you need more information.

Thanks & Best Regards