MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ASM330LHH

While I’m using ASM330LHH the gyroscope’s data jump to unusual value just once sometimes . The data rate is 10hz 

IMG_1599.jpeg
Mal by Associate
  • 796 Views
  • 1 replies
  • 0 kudos

LSM6DS032 programming finite state machine

Hi all, I'm trying to move Finite State Machine config from devkit using Unico GUI to final application. I've prepared movement wakeup example from FSM datasheet in Unico, which is working totally fine on devkit, it could even detect knocking in desk...

Zrzut ekranu 2024-02-05 113640.png
mpopko by Associate II
  • 2828 Views
  • 5 replies
  • 0 kudos

IIS2DH INT1 signal generation

Posted on June 12, 2017 at 11:07Hi,I have inserted the accelerometer in a custom board.Is is connected via I2C to a microcontroller, Vdd and Vdd_IO both connected to 3V3.In my application the micro controller awakes when the acceleration on all the ...

Magnetometer output seem false (IIS2MDC)

Hi everyone,   First of all, I use a STWINBX1 board, which include a MCU and several sensors. I try to get the magnetic field by reading the output of the magnetometer (IIS2MDC), but the output value seems false. Please note that : - I checked the PI...

Resolved! LSM6DSO Int2 on Int1although it is disabled

Hi,we are using the LSM6DSO in Fifo mode and with the double tap feature. Our firmware configures the Sensor Frontend to give an interrupt at fifo_th on INT1 and for double_tap on INT2. Therefore, we explicitly disabled the INT2_on_INT1 bit inside th...

SCR01.PNG
CWies.1 by Associate III
  • 1638 Views
  • 4 replies
  • 0 kudos

Resolved! LPS28DFW vibration susceptibility

Hello,I am wondering if the presence of gel in the LPS28DFW makes it more susceptible to vibration than LPS22DF. These sensors will be in a vibration environment, and I'm concerned that the vibrating gel in the sensor will negatively affect the press...

VCu by Associate
  • 1023 Views
  • 2 replies
  • 0 kudos

LIS3DH: FIFO configuration freezes acceleration readings

Hello all,I want to use FIFO to store my acceleration data.When FIFO is not configured, the data I read from OUT_X_L, OUT_X_H, OUT_Y_L, OUT_Y_H, OUT_Z_L, OUT_Z_H are okay. By "not configured" I mean FIFO_CTRL_REG = 0x00, which is the default value th...

STHS34PF80 - cover glass

Hi,we are working on integrating this sensor to our device. We would like to make it work as human detection in front of our device. I am testing this sensor using "STEVAL-MKI231KA" board without lens connected to our development board via I2C and I ...

rfi by Associate
  • 1189 Views
  • 2 replies
  • 1 kudos