MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I reset the fifo in the LIS2DH12

I need to clear the fifo and then at a later time read all samples taken since then.  Then later I will repeat this. I don't want any samples before or after that time window to get in my data.  I looked through the library and I can't see anything t...

mchahn by Senior
  • 1006 Views
  • 1 replies
  • 1 kudos

Resolved! Unico GUI cannot communicate with MKI109V3 Board in Ubuntu 18.04

Hi, I am using MKI109V3 as motherboard and MKI239A as IMU adapter. My Unico version is 9.16. Following UM2116, I tried everything in Windows 10, including firmware upgrade to 3.58.2 (latest), and all data display works fine in Unico.After that, I wan...

ZSong by Associate III
  • 2165 Views
  • 4 replies
  • 1 kudos

Resolved! Spikes in ASM330LHH Temperature Data

Hi, I am currently using an ASM330LHH MEMS, and seem to be getting erroneous spikes in data from the temperature sensor (see attached image). Please can someone advise on what this may be, or if you have experienced the same issue? I have been workin...

M_S by Associate II
  • 2190 Views
  • 5 replies
  • 4 kudos

lis3dh -6d orientation

hey there,Im trying to use lis3dh in low power consumption mode and hope to get advices on how to use the interrupt and the registers set up for minimum power consumption aiming to few micros.

Mor45 by Associate
  • 619 Views
  • 1 replies
  • 0 kudos

MP23DB02MM Frequency Range

I interested in the higher frequency range of this device. The datasheet states clearly the LF cutoff at 35Hz, but there is no real discussion on the HF end apart from the characteristic graphs stopping at 10KHz. The device can be clocked up to 3.3MH...

JKing.3 by Associate II
  • 1399 Views
  • 5 replies
  • 0 kudos

Resolved! LSM6DSO master I2C pull up resistors

Hi @Eleon BORLINI, I am trying to build a custom 9 dof imu using LSM6DSO and LIS3MDL in mode 2, according to LSM6DSO datasheet.I found this page on AN5192 about sensor mode 2 (pg. 63). i2c master would be LSM6DSO and i2c slave would be LIS3MDL in thi...

el659_0-1703026493960.png
el659 by Associate III
  • 950 Views
  • 1 replies
  • 1 kudos

Resolved! A problem about ASM330LHB safety lib

Hello,     I have applied for the ASM330LHBxx ASIL B library from ST's web, and integrated it to my program, all the functions worked fine. But the noise of GYRO has gone beyond our requirement, we used to enable the LPF in ASM330 to lower the noise....

ssdgf by Associate
  • 2015 Views
  • 3 replies
  • 0 kudos

LPS28DFW arduino

Hello,Actually i'm trying to mesure the pressure using LPS28DFW and arduino uno, but i have some problems, the i2c communication does not working.Can help me please and thank you.arduino code : #include <Wire.h>#include "SparkFun_LPS28DFW_Arduino_Lib...

ljm by Associate III
  • 1166 Views
  • 2 replies
  • 0 kudos

orientation and movement values in LIS2DW12 accelerometer

Hello We are working with accelerometer LIS2DW12.we did tests on the different movements of the accelerometer and the graphs we see (the graphs were made with the x_physical y_physical z_physical values). However we see graphs that are not as we expe...

0693W00000BbSy9QAF.jpg 0693W00000BbT1GQAV.jpg 0693W00000BbT2OQAV.jpg 0693W00000BbT2iQAF.jpg
Msaga.1 by Associate II
  • 3946 Views
  • 25 replies
  • 0 kudos