MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Asm330Lhh DEVICE_CONF

Hello, I have encountered some issues while developing with the  ASM330LHH. During the initialization sequence of the ASM330LHH interface, I first read the WHO_AM_I  register. After confirming that the value is correct, I proceed to access other regi...

wz2 by Associate
  • 208 Views
  • 2 replies
  • 0 kudos

Resolved! LIS3MDL calibration issues

I'm using a LIS3MDL magnetometer on my board, and I figured out how to calibrate it to account for distortions  caused by the board, and the procedure works. However, it seems that every time the same magnetometer is turned off and re-powered, the me...

bu by Associate
  • 190 Views
  • 1 replies
  • 0 kudos

Resolved! ST1VAFE3BX vAFE validation against reference signals

I'd like to validate ST1VAFE3BX vAFE measurement data against test signals as part of hardware design validation of a custom ECG sensor design based on ST1VAFE3BX. I intend to input reference signals (differential or single ended) into the two bio ch...

bwilkins by Associate II
  • 763 Views
  • 6 replies
  • 0 kudos

LIS2MDL (LGA-12L) Leakage current

Hi Team,We have designed and manufactured several thousand PCBs that include the LIS2MDL (LGA‑12L) sensor. All boards are functioning correctly from an operational standpoint. However, because our devices run on battery power, load current is critica...

Mallik18 by Associate II
  • 557 Views
  • 8 replies
  • 2 kudos

Microphone self noise IMP34DT05

Hello,I'm using the IMP34DT05 microphone and it records fine but there is always a noise overlapped and it is very annoying.I have tried recording the background noise in anechoic chamber (see attached audio, high-pass filter alpha is 0.98). Do you k...

frnt by Senior
  • 2309 Views
  • 3 replies
  • 0 kudos

Resolved! I2C with IMS330dlc

Hi I am new to the I2C communications. I am trying to communicate to the IMS330dlc chip. I am using a lab jack U3-HV.. I am programming this via Visual Studio 2022 using c# code. I cant get back the 106 for Who am I. below is the code that I setup on...