cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to run FIFO data and MLC at the same time for the lsm6dsv16x?

ACand.3
Associate III

I followed most of the examples to get data such as accel, gyro, timestamp and temperature from the github repo using fifo interrupts. I also used the mlc_gym example to get data from a MLC configuration that I designed on Mems studio. 

 

My question is, can I use both configurations at the same time? like have an interrupt for the fifo data ready and one interrupt for the MLC? 

As in, I am constantly reading raw accel/gyro/timestamp/temp data at a fixed 60Hz on interrupt 1 and also get a new MLC state on interrupt 2?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ACand.3 ,

Yes, you can use an interrupt for the FIFO and the other one for the MLC at the same time.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @ACand.3 ,

Yes, you can use an interrupt for the FIFO and the other one for the MLC at the same time.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.